Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
The Topology search is particularly suitable where single attributes such as Size, Distances, Angle, Pattern, etc. are possibly more characteristic than the form. It can be used without textual information and without reference part. It also can be used in searching out the best part step by step when result parts provide (new) search terms via part information or can serve as reference part for a following geometrical search.
Topology search here, exemplarily with the search conditions Circular pattern (Number of patterns: 1) and Symmetry (Rotation symmetry: symmetric)
In the opened menu of the enhanced search methods, click on Topology search.
Click on the respective button.
-> The search condition is displayed with the respective parameters below.
Then click on the desired parameter(s) and confirm by clicking on the green checkmark.
You can add as many conditions as you like. And you can search just with one condition.
-> Selection is displayed in the dialog area of search methods.
-> The results are listed on their own tabbed page. When moving the mouse over a result, you can check the part in 3D.