Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
The functions for automatic alignment are found in the 3D comparison section top left in the toolbar:
|
|
Overlay components : Possibly the functions Original rotation and centered position and Original rotation and position more effective.
|
|
Automatically calculate aligned rotation and position: Is according to the context menu command Center parts. |
|
Original rotation and centered position (best fit)
In the side view you can see, that the parts are not 100% identic.
In the section view you can optimally see the differences. See Section 3.1.6.10.3.1.1, “Part comparison in sectional plane ”. |
|
The button corresponds to the functions of orientation of parts or takes effect if parts have been manually moved or rotated. With Undo you can restore the last position. |
|
Expert mode: With click on the button at the left side a section with the Oppose, Overlay and Colors/Transparency index pages is displayed.
Detailed information on this is found under Section 3.1.6.10.3.2, “ Expert mode ”. |
In the context menu of 3D comparison you can find the following menu items:
In the sectional plane the part differences are quite clear at a glance.
A detailed description of the functionality is found under Section 3.1.6.10.3.1.1, “Part comparison in sectional plane ”.
Measuring grid [68]
Select a sectional plane and the desired offset from zero plane.
Click on the respective button in the toolbar or alternatively on the command Define section cut... in the context menu of the 3D window.
After calling the function a navigation cross with 6 arrows is displayed.
See Section 3.1.6.10.3.5, “ Colors/Transparency tabbed page ”.