powered by CADENAS

Manual

Manual

5.3.3. Move part in flute

The view under Details automatically switches to the dialog for the selection of the position on the add line.

Determine assembly position for part

Determine assembly position for part

Part 2 inserted

Part 2 inserted

These are the following options for positioning:

  • Free entry of value in marked field (default value is the starting point)

  • Beginning

  • Middle

  • End

Confirm with OK.

--> The part is accordingly positioned on the add line. (In this example, the "Beginning" position was kept)

[Note] Note

After inserting a part the dialog for positioning on the connection line pops up automatically.

Via the Move part in flute button you can open the dialog at any time.