Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
Using the Variables search you can search for values of certain variables.
ERP variables are always displayed in the dialog box (when using an ERP integration) and also classified variables like CNSORDERNO (order number).[45] With these variables you can search catalog-spanning.
Furthermore the common geometrical variables of a selected directory level are displayed. The above figure is exemplarily showing the common variables of Standards -> ISO -> Bolts.
In the opened menu of enhanced search methods, click on Variables search.
Determine the logical operator.
= equal > greater < smaller >= greater or equal <= smaller or equal x-y from to
Optionally, you can manually add variables.
After clicking on Add variable, an empty row is added. Enter variable name and value. By clicking on the entry can be removed again.
-> The selection is displayed in the dialog area of search methods.
When searching for a class system variable, the column Class system values is displayed (if activated in the Properties dialog [right mouse key over column header]).
Common variables are also displayed in the dialog area Suggestions. On this also see Section 3.1.6.4.3.2, “ Variables search: Call from dialog area "Suggestions"”.
The Filter Assistant is also based on these common variables. On this also see Section 3.1.6.4.12.1, “Quick filter search with auto filter”.
[45] The displayed class system variables are set by the administration via config key. On this see Section 1.7.5.19.2, “ Block [VARSEARCHCLSVARS]” in PARTsolutions / PARTcommunity4Enterprise - Administration Manual.