powered by CADENAS

Manual

Manual

3.1.14.3.2. Result list

In the report Search finished parts for unmachined part the result list shows finished parts, which can be produced from the unmachined part.

In the report Search unmachined parts for finished part the result list shows unmachined parts, from which the finished product can be produced.

In the exemplary figure the Waste is 4,2%.Waste

In the exemplary figure the Waste is 4,2%.

Waste: Waste volume of the unmachined part (compare settings dialog: Maximum waste in unmachined part)

Protrusion: Missing volume in the unmachined part (compare settings dialog: Accepted error in finished part)

The volume is displayed in addition to the percentage value.

Parts from the result list do not have to be absolutely opened, because 6 preview images depict the respective part from all sides and volume errors are marked in red.

This is very useful information, because the part is not yet assembled and another unmachined part from the stock can possibly be used. The report delivers all needed information.