powered by CADENAS

Manual

Manual

3.1.14.3.1. Settings

The setting options for Search unmachined parts for finished part and Search finished parts for unmachined part are identic.

Search unmachined parts for finished part

Search unmachined parts for finished part

Search finished parts for unmachined part

Search finished parts for unmachined part

  • Search sample (finished part) / Search sample (unmachined part)

    • Use selected part: Select the desired part in the index tree.

      [Note] Note

      NOT the part used in the 3D view is used!

    • Load file: Select the desired part via browse button ....

  • Number of search results

  • Accepted error in finished part

    The error is caused by "missing material" on the unmachined part.

  • Maximum waste in unmachined part

    The maximum waste defines, how much material is allowed to be removed.

  • Resolution

    The resolution controls the search quality. With higher resolution more details are covered, however the search takes more time.

  • Filter for result list:

    A Search for unmachined parts can be combined with a Variables search. Under Section 3.1.14.3.1.2.1, “Example - Search for unmachined parts combined with Variables search ” you can find an example on this.

    Detailed information on Variables search is found under Section 3.1.6.4.3, “ Variables search ”.

  • Search only in preferred rows

    It is also possible to create a report based on preferred parts. Therefor activate the checkbox. This is according to the activation of the button Preferred rows on/off in the ERP toolbar. Then the report only uses preferred parts.

    [Note] Note

    The on/off state of the button Preferred rows on/off in the ERP toolbar is irrelevant for reports.

  • Unmachined parts to search or Finished parts to search

    At directories to be searched select the checkbox.