powered by CADENAS

Manual

Manual

6.8.  3D preview

No display or affected display

Virtually all PARTsolutions modules feature 3D previews. This allows you to visualize components or assemblies before exporting them to your CAD system.

However, certain graphics adapters do not support rendered display for the 3D preview in the PARTsolutions modules. Consequently, the 3D display (resolution or sequences of motion) is impaired in a PARTsolutions module. You can make the following corrective settings in the GUI in order to eliminate or reduce these errors.

Open the Options menu via Extras, Settings... and click on the 3D view.

Check the Software rendering option button so that the 3D display is "software-driven" (Open GL, Windows). This is because Software Rendering stands for a reliable display mode which may sometimes not be so "demanding".

[Note] Note

Saved settings:

If you delete the CADENAS-settings which you have made (e.g. Cadenas (high quality)), it is not possible to restore them!

[Note] Note

The cause for poor quality of depiction (for example line thickness of the edges and threads), may also have to do with the operating system.

Check if the color quality is set to 32 Bit under Windows -> Desktop -> Settings.