Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
On the License selection tabbed page in floating installations you can determine, which PARTsolutions license packages you want to use in the current application. Normally this is preconfigured during the installation or by your product support. However it may be necessary to dynamically change it, if you want to use the product in different functionality.[138]
You have the following options:
Overwrite license preselection:
If you want to change or overwrite the administrative preselection, then activate the Overwrite license preselection option.
For each single license product you can open a list field by double-clicking on the displayed Status. Clicking on the arrow key the whole list becomes visible. Select the desired Status.
Suppress the interactive product selection dialog...
You have the following options:
Activation and selection of the desired license product from the list field:
-> When the module launches no selection box will display and the chosen license product is automatically used.
-> When the module launches the selection box appears according to the administrative preselections or according to the settings made here in the Overwrite license preselection list field.
Take the currently running modules into account for the automatic preselection
Example: Assumed PARTproject is already running, then a license is used, which is able to provide this module with a respective license.
Take licenses taken by other modules into account for the automatic preselection.
Example: PARTproject already uses a certain license. Then for PARTdataManager the same license is used, although theoretically another license would have been possible alternatively.
Enable to pull other base products during program runtime when they are needed