powered by CADENAS

Manual

Manual

3.1.3.2.2.3.  Meta file batch

With the Meta file batch command, the row content (table) of the selected part is transferred into a Destination directory of your choice as a meta file.

Via %LINE% the row number is extracted and enables the singular identification as well as the listing of the individual rows.

In the Programs to start field, set the program that should be opened and the respective row content, if needed "continue processing". %DIR% pulls up the last transferred file, %NAME% takes over the name of that file. If the option Prompt for each file is activated, the program with every transferred row restarts every time, otherwise the launch takes place only once at the end of the batch.

In the Log file field you can apply a directory into which corresponding protocols can be entered in case of errors.