powered by CADENAS

Manual

Manual

3.1.1.6.10.2.  Tabular Compare

The table view shows the comparison for:

  • ERP data (if available)

  • Classification data

  • Topology

  • Parameter of geometry

[Note] Note

Divergent table values between the single parts show a red background color.

Topological parameters are color-marked so that you can see the most important ones at a glance.

Topological parameters under "Search results"

Topological parameters under "Search results"

Topological parameters in the "Part comparison"

Topological parameters in the "Part comparison"

  • Explicitly searched topological attributes are marked in orange color by default, as it is in the search results.

  • Those topological parameters which can be marked in the 3D view (Inner cylinders, Outer cylinders for example), have a checkbox in the listing under Tabular Compare.

    If you activate a checkbox then the respective parameter is color-marked both in the Tabular Compare and in the 3D comparison. Different parameters get different colors (regardless of whether they have been automatically or manually marked)

Icons

In the column header you can find the following icons:

Select project line (see identic context menu command) -> The table is opened.

Select as master: The respective column is displayed with green background color.

Load as first project (in the 3D, 2D comparison)

Load as second project (in the 3D, 2D comparison)

Open selected line in PARTdataManager

First select the desired row in the Select project line dialog.

Export to CAD:

First select the desired row in the Select project line dialog.

Geometric similarity

At parts, which are found via Geometric search (3D) and are transferred into the Part comparison, there, in the Tabular Compare section the geometric similarity is overtaken and displayed as well.[54]

Context menu

Open: Right-click anywhere in the desired column.

Tabular Compare - Context menu commands

Tabular Compare - Context menu commands

In the context menu the following commands are available:

  • Select as master [compare icon above ]

    The corresponding column is displayed with a green background color.

  • Load as first project (in the 3D, 2D comparison) [compare icon above ]

  • Load as second project (in the 3D, 2D comparison) [compare icon above ]

  • Select project line [compare icon above ]

    Switches to the row view (see following figure)

    By clicking on Back, the display changes to the export state.

    For a logical 3D comparison, change the properties so that the compared parts possess about the same dimension.

    Tabular Compare - row view

    Tabular Compare - row view

  • Remove project

    Removes the selected project from the "Tabular Compare" section.

  • Unselect all topological features

    For example, at the topology search markings according to the search parameters are automatically set. You can easy remove these all at once with this command.

  • Open 3D file...

    Load any native file (specific CAD file or neutral format) in the Compare dialog.

    [Note] Note

    Precondition: The CAD system has to be started.

    1. Click on the menu item Open 3D file....

      -> An Explorer window opens.

    2. Browse to the desired file.

      A number of formats can be opened: [55]

      A selection of formats:

      • IGS (*.igs)

      • STL (*.stl)

      • Inventor 2010 (*.ipt, *.iam)

      • NAT (*.nat)

      • PS3-V2 3D (*.ps3)

      • PartJava 3D (*.zjv)

      • Pro/Engineer Wildfire version 3 32 Assembly (*.asm)

      • Pro/Engineer Wildfire version 3 32 Part (*.prt)

      • Pro/Engineer Wildfire version 3 32 UDF (*.gph)

      • SAT ascii 3D (*.sat)

      • STEP (*.step, *.stp)

      • SolidDesigner PKG File (*.pkg)

      • SolidDesigner PKG/STL File (*.stl)

      • Solidworks 2010 (*.sldprt, *.sldasm)

      • U3D (*.u3d)

      • *.zjv

      [Note] Note

      Make sure that when selecting CAD formats, the CAD application has been started.

    3. If there is an ambiguity for a file extension, an additional dialog box appears.

      Ambiguities are possible for a file extension such as .prt for example, which is used by Creo Elements and NX as well, furthermore for several versions of a CAD system.

      In the list field select the desired system and the desired version.

    4. Then the dialog box Selection for unit opens.

      In the list field, select the correct unit: mm, cm, dm , m, INCH, FEET, INCH/10, INCH/100

      Confirm by clicking on OK.

      -> The file is loaded in the Tabular Compare section.

  • Remove all projects

    Removes all projects from the "Tabular Compare" section.

  • Copy (only displayed over table cells)

    Open the context menu via the desired table row and select the Copy command.

    Now you can insert the cell content in a text editor.

  • Print

    The complete table is printed.

  • Pin name column | Pin description column | Pin preview header

    In order to keep in view the important during vertical and horizontal scrolling, it possibly makes sense to fix the columns "Symbol" and/or "Description" [horizontal scrolling] and/or the complete preview line [vertical scrolling].

    In the Tabular Compare section call the context menu and activate the desired option.



[54] You can configure, whether the geometric similarity shall be displayed. See Section 1.1.6.6.4.2.1, “ Key "DisplayGeoDistances" - Tabular Compare - Display geometric similarity ” in PARTsolutions / PARTcommunity4Enterprise - Administration Manual.

[55] The number depends on the installed CAD systems.