powered by CADENAS

Manual

Manual

3.1.2.4.6.1. Context menu of an assembly

Right-click on the name of the assembly in the Assembly dialog box.

--> The respective context menu opens.

3.1.2.4.6.1.1.  Search...

Option Text search:

This searches the assembly for a term, an abbreviation.

Under Search in you can choose:

  • Parts

  • Connection points

  • Parts and connection points

--> All elements that contain the search term will be listed.

If you click on a search result, the PARTdataManager jumps to the respective spot in the Assembly.

Option Error:

After assembly construction this searched for elements that have not yet been uniquely determined (table rows not yet selected).

--> All elements that contain the search term will be listed.

If you click on a search result, the PARTdataManager jumps to the respective spot in the Assembly.

3.1.2.4.6.1.2.  Transparency

  • Transparency : Regulate the transparency of a body

    • fully visible

    • 25%

    • 50%

    • 75%

    • invisible

    • configure transparency... (See figure at right)

      Via the sliding controller you can set the transparency continuously.

3.1.2.4.6.1.3. Insert part

Insert ... transfers the respective part into the Assembly.