powered by CADENAS

Manual

Manual

3.1.2.1.2.5. Export "Others" formats

3.1.2.1.2.5.1. Export in AVI format

Make the settings on the below described AVI options and Cross-section tabbed pages:

Export in AVI format

Export in AVI format

Tabbed page AVI options

  • Picture settings:

    Width in pixel, Height in pixel

    Into the input areas, enter the desired height and width.

  • Animation settings:

    • View:

      In the list field, select the desired view:

      • Front

      • Back

      • Right

      • Left

      • Top

      • Bottom

      • Isometric

    • Bitmap format:

      Usually leave the default value "RGB32".

      Otherwise select the desired bitmap format from the list field.

    • Animation frame:

      Frames per rotation

      [Note] Note

      Please note the interaction of the settings under Rotation settings.

      Example:

      If you set a rotation step to 1°, you will need 360 frames per rotation, so that a full rotation may be carried out.

      The more frames, the larger the file.

    • Delay between frames in 1/100 secs. (1-255)

      The rotation speed is a result from this setting and the Animation frame setting.

    • 3D template:

      You can adjust the color style to the layout of PARTsolutions versions, CAD systems and other style sheets:

      8.1, 9.0, Purist, Metal, Wood, Catia V5, Solid Edge, SolidWorks, NX, One Space Designer, Pro/Engineer, Inventor

    • Transparency:

      In order to get a transparent background, activate this option.

      Not transparent

      Not transparent

      Transparent

      Transparent

  • Codec configuration:

    • Codec

      From the list field select the desired Codec.

      [Note] Note

      The list values are not set, they are read out from your system.

      The setting No Codec offers the best quality. However, without Codec you get very large files.

      Select a Codec from the list with which the quality and file size are in the desired relationship.

    • Scale: Default value '1' (lowest possible value)

      Time scaling. The larger the number, the slower the movement.

    • Frames per second: 24

      The more frames per second, the smoother the movement, but also the larger the file.

    • Bytes per second: Default = 500

      This setting concerns the quality

    • Quality (0 - 10): Default: 10

      General settings for quality

    • Keyframes: Default value =1

      Usually you leave this setting. Changing to '2' would cut the number of key frames in half.

    • Interleaving:

      Audio and video data is saved meshed together.

  • Rotation settings:

    Optionally, you can define the rotational increment in degrees for individual axes.

  • Destination file:

    Via Browse ... the Explorer opens.

    If desired, change the path and the file name. Either way be sure to leave the file ending.

Tabbed page Cross section

  • Cross-section

    Cut plane:

    From the list field, select the YZ plane, XZ plane or XY plane

    '+' or '-' (mirror inverted display of cut)

    Displacement of cut plane

    In the input field, enter the desired displacement. (The numerical value refers to the measuring unit of the part.)

  • Quarter cut

    In order to create a quarter cut, activate both the selection box at Cross-section, as well as at Quarter cut.

    The same things apply as for the settings of cross section.

Cross section

Cross section

Quarter cut

Quarter cut

3.1.2.1.2.5.2. Export PDF (U3D) format

All parts from CADENAS catalogs can be displayed as 3D solids in the widespread Adobe PDF format. Parts ad assemblies can thus be displayed in 3D on all computers worldwide with a free standard license from Adobe Acrobat Reader (as of version 7.0.8). It is therefore possible to get a realistic view of the part prior to purchasing it.

The application range of Adobe Acrobat 3D are 3D processes of coordination, in other words better cooperation with technical documents through the integration of 3D data, shorter development times due to clearer 3D designs and the avoidance of construction errors. A further area of use is the technical documentation. The 3D design data can now be displayed on any desktop without the use of CAD applications and the preparation of the CAD data for marketing and technical documentation is easy as pie.

Compare also Section 3.1.2.1.2.5.3, “Export PDF datasheet ”.

Via the Export menu, or the respective toolbar, select File -> Others -> PDF (Only 3D).

-> The Export in PDF (Only 3D) format window opens.

Some setting options of the Acrobat Reader can be performed in the dialog box.

Under Destination file, define the name and storage location of the file.

Details on the tabbed page Export Options can be found under Section 3.1.2.1.2.5.6.1, “"Export options" tabbed page -> Export accuracy ”.

Open the PDF file.

3D PDF in Acrobat Reader

3D PDF in Acrobat Reader

License

In order to be able to export CADENAS parts from PARTsolutions as 3D PDF, you need a license for the Acrobat interface,but not a full license for Adobe Acrobat 3D.

3.1.2.1.2.5.3. Export PDF datasheet
3.1.2.1.2.5.3.1. Application

The 3D PDF data sheet was developed for the platforms PARTcommunity, PARTserver and PARTsolutions (as of V8.1.08) (as well as Offline CDs). Using the data sheet function, a 3D PDF document can be created from an online catalog or from a local installation. The view can contain a 3D model, 2D view with dimensioning and photo-realistic images, a characteristic attribute table, and many more characteristics.

  • Important for catalog manufacturers is that no changes must be made to the catalogs when creating 3D PDF data sheets, because the data sheet is automatically loaded into the already existing eCATALOGsolutions catalog data.

  • Due to the unique data sheet definition, the 3D PDF data sheet is mainly interesting for the end user. All catalogs at all PARTsolutions workstations produce identical worksheets which drastically improves internal documentation. In addition, all 3D PDF data sheet users receive all information in an summary which greatly supports product selection.

  • After creating the 3D model the data sheet is immediately available and through the support of the 3D function, exhibits and innovative method with a low error rate.

  • The 3D PDF data sheet is available in several languages for PARTcommunity, PARTserver, PARTsolutions and Offline CDs.

3.1.2.1.2.5.3.2. Settings

In order to create the 3D PDF data sheet, a layout template must be defined. This contains information on how the data should be arranged on the PDF.

[Note] Note

A standard template or a company template according to the corporate design may be used.

You can create your company template via PARTtemplateDesigner yourself or commission CANVAS, CADENAS' own marketing agency.

The CADENAS standard template does not include a 2D derivation, for example. It is however possible at all times to create templates with 2D derivation.

The templates are filled with Standard text, Standard number, preview images, U3D image (interactive 3D view),[83] technical previews, 2D derivations, table values, etc.

Adobe Acrobat Reader Version 8.x is recommended when using 3D functionality.

All displays correspond to the table row chosen during export.

CADENAS standard template

CADENAS standard template

Company-specific template - Example 1

Company-specific template - Example 1

Company specific-template - Example 2

Company specific-template - Example 2

In the PDF data sheet the option Shaded view can also be selected for the 2D derivation. The creation is much quicker and is a good alternative, because no real line depiction is needed.[84]

Template specific to the company - Shaded view

Template specific to the company - Shaded view

You can display the Windows user name and the mass of the part/assembly in the PDF data sheet. The mass declaration is important among others, in order to be able to calculate the carrying charge. The user name is interesting for company internal data sheets e.g. at incoming orders, when the data sheet is enclosed to the order.

  1. Open the export format in PARTdataManager via the icon PDF Datasheet .

    -> The dialog box Export in PDF datasheet format opens onto the PDF export options tabbed page.

  2. Select template

    The standard selection Use default-template is activated.

    [Note] Note

    Leave the activation alone. For all standard cases the setting is correct.

    If company standard templates are available for the currently selected catalog, you may select these from the list field Plane, otherwise please select Cadenas.

    Derivation view Select

    [Note] Note

    This setting is only relevant if the template stipulates the display of a 2D derivation.

    • Overwrite derivation view from template:

      • Is the option set, the setting is under Derivation view in the list field will be used.

      • Is the option not set, the presetting from the template will be used independent of the setting under Derivation view. If no presetting has been made in the template then the setting under Derivation view in the list field will also be used.

    • Derivation view:

      • 2D derivation

      • 2D-Derivation

      • Shaded View

    • Open generated datasheet (optional)

  3. Via Browse ... set the path to the Destination file.

  4. Table tabbed page -> Remove column from table:

    On the Table tabbed page you can remove columns from the table for the data sheet view. Activate the checkbox for all columns which you do not want to be displayed.

    • Under Export options optionally adjust the Export accuracy.

      In the list field select the desired accuracy:

      • Current selection

      • Low

      • Medium

      • High

      • Very high

      The part is calculated with the set level of detail before the export.

      This function is identic with the level of detail option in PARTdataManager, but here only temporarily for the export.

    3.1.2.1.2.5.4. Export QR code

    QR code (Quick Response) is available as export format.

    Troublesome typing of links and information is not necessary anymore.

    This feature can well be used in print catalogs. So CAD models can directly be downloaded from a print catalog in one single step.

    In order to export the QR Code for a single project proceed as follows:

    Call: Export menu -> Export in file -> Others -> QR Code

    Export format: QR Code

    Export format: QR Code

    Settings on tabbed page QR options:

    Information used in the input fields Base link, Link options and Text are embedded in the code. Part parameters such as $NN., $NT., $NB., $ALL_VISCOL. (all visible parameters), $ALL_COL. (all parameters), $ProjectPath. (project path) can be used.

    There are two basic settings:

    • PARTcommunity link:

      If PARTcommunity link is selected, then base link, project path and link options are automatically combined.

      Examples:

      • Link PARTcommunity project

        Entry under Base link:

        http://b2b.partcommunity.com?info=

        No entry under Link options:

      • Link PARTcommunity project and line

        Entry under Base link:

        http://b2b.partcommunity.com?info=

        Entry under Link options:

        &varset={$ALL_VISCOL.}

    • Text:

      If Text is selected you can create any combination. This may be links or other texts as well, which shall be saved in the QR.

      Example:

      Link to your own home page with order number BNR (from table)

      http://www.my_company.com/showproject.asp?NR=$BNR.

    Settings on tabbed page Export Options: See Section 3.1.2.1.2.5.6.1, “"Export options" tabbed page -> Export accuracy ”.

    Batch export

    You can export the QR Code for complete directories:

    • Call up PARTdataManager

      Right-click on the index tree -> Generate image data/preview images

    • Call up PARTproject

      Right-click in the index tree -> Output -> Generate image data/preview images -> export mode Export files

      (The dialog is the same like under PARTdataManager, but here no preview image is displayed.)

    -> The Export files dialog box opens.

    Select the export mode Export files.

    "Default options" tabbed page

    "Default options" tabbed page

    Select the format QR Code.

    "View / Export" tabbed page

    "View / Export" tabbed page

    Under Export select the target path and possibly adjust the presettings under Name of exported files.

    3.1.2.1.2.5.5. eClass Advanced

    If in a pre-process eClass Advanced attributes has been enclosed in the project you can now export this information in the form of a XML file.

    "Export" menu -> "Export in file" -> "Others" -> "eClass Advanced"

    "Export" menu -> "Export in file" -> "Others" -> "eClass Advanced"

    -> The respective XML file enclosed to the project is exported.

    Excerpt from XML file:

    ... 
    <FEATURE>
           <FTEMPLATE>
               <FT_ID>0173-1#02-BAD291#007</FT_ID>
               <FT_NAME>Direktmontage möglich</FT_NAME>
            </FTEMPLATE>
            <VALUE_IDREF>0173-1#07-CAA017#002</VALUE_IDREF>
            <FVALUE_DETAILS>Nein</FVALUE_DETAILS>
            <FID>323</FID>
            <FPARENT_ID>-1</FPARENT_ID>
    </FEATURE>
    ...

    Details on how to import eClass Advanced information can be found under Section 4.7.2.1.15.2, “ Import eClass XML file... ” in eCATALOGsolutions Manual.

    3.1.2.1.2.5.6. Export further "Others" formats

    Export formats "Others"

    Export formats "Others"

    In this section you can find the following formats of the Others menu item. At each format the available tabbed pages are listed, where you can perform settings. With click on the link you will reach the respective section.

    3.1.2.1.2.5.6.1. "Export options" tabbed page -> Export accuracy

    On the Export options tabbed page you can adjust the Export accuracy.

    Export accuracy

    Export accuracy

    In the list field select the desired accuracy:

    • Current selection

    • Low

    • Medium

    • High

    • Very high

    Before the export the part is calculated with the set level of detail.

    The function is identic to the level of detail option in PARTdataManager, but here only temporarily for the export.

    3.1.2.1.2.5.6.2. "Cross-section" tabbed page

    Cut part

    • Cross-section

      Cut plane:

      In the list field, select YZ plane, XZ plane or XY plane

      + or - (mirror-inverted display of cut)

      Displacement of sectional plane:

      In the input field, enter the desired displacement. (The numerical value corresponds to the measuring unit of the part.)

    "Cross-section" tabbed page

    "Cross-section" tabbed page

    • Quarter cut

      In order to create a quarter cut, activate both the checkbox at Cross-section, as well as at Quarter cut.

      The settings are the same as for a cross section.

      Cross section

      Cross section

      Quarter cut

      Quarter cut

    3.1.2.1.2.5.6.3. "Transformation" tabbed page

    On the tabbed page Transformation, you can adjust the axis orientation and scaling for the exported part.

    3.1.2.1.2.5.6.4. "Reduction" tabbed page

    On the tabbed page Reduction, you can not only specify a certain number of triangles, but also the required result quality.

    • Default: Reduces to the predefined number of triangles. If the current number of triangles undershoots the predefined count, no reduction will be made.

    • Light: Light reduction. Great for a simple reduction of the face count of Parts. The topology will not be changed. Circles will be approximated by many faces.

    • Medium: Medium reduction. Great reduction of the face count of any Part. The topology will not be changed. Circles will be approximated by less faces.

    • Rough: Rough reduction. Great reduction of the face count of big or highly triangulated parts. Can destroy the topology of small parts and can lead to edged circles.

    3.1.2.1.2.5.6.5. "Filter" -> Geometry tabbed page

    In the Geometry section you can perform the following settings optionally:

    • Export draft as sweep:

    • Split pattern:

    • Convert holes:

    "Filter" -> Geometry tabbed page

    "Filter" -> Geometry tabbed page

    3.1.2.1.2.5.6.6. "Collada options " tabbed page

    On this tabbed page you can perform settings for Lightning and Scale.

    Collada options

    Collada options

    3.1.2.1.2.5.6.7. "WebGL Html" tabbed page

    WebGL (Web Graphics Library) is a JavaScript API for rendering interactive 3D computer graphics and 2D graphics within any compatible web browser without the use of plug-ins.

    Settings:

    Choose the desired top and bottom background color.

    Optionally, create a hyperlink. The Hyperlink text is displayed on the webpage centered at the top.

    Adjust the settings under Base link as needed.

    When selecting the Text option you can specify free text in the Text input field.

    HTML result:



    [83] For use of 3D functionality, Adobe Acrobat Reader is recommended as of Version 8.x.

    [84] As of 9.03 SP2