powered by CADENAS

Manual

Manual

3.1.3.3.2.4.  Table

This table shows all values and sizes of the current part.

3.1.3.3.2.4.1. Table areas - Functions - Overview

3.1.3.3.2.4.2.  Choose display range

  1. A click on the title of a column opens the window Choose display range. In the fields you can set a Value or Categories , which restricts the display of the table. Please make sure that you only enter sensible settings (digits)! It is also possible to Sort Ascending/Descending.

  2. Remove filter:

    A right-click removes this "filter".

    --> The entire table becomes visible again.

  3. Remove filter:

    Right-clicking into the field at the top left, removes several restrictions within the table.

3.1.3.3.2.4.3.  3D preview

In the 3D preview, always that part is shown which you have just marked in the table.

3.1.3.3.2.4.4.  Restrict table

Another opportunity to restrict the displayed range of table, is to point out one value. In the example the value CL-200-VTC is clicked on. → The table will be reduced (e.g. column B for "Width" to value 6.000) so that only parts with this PARTNO are displayed. This restriction is removed as mentioned.