powered by CADENAS

Manual

Manual

3.1.2.3.3.1. Settings

The setting options for Search unmachined parts for finished part and Search finished parts for unmachined part are identic.

Search unmachined parts for finished part

Search unmachined parts for finished part

Search finished parts for unmachined part

Search finished parts for unmachined part

  • Search sample (finished part) / Search sample (unmachined part)

    • Use selected part: Select the desired part in the index tree.

      [Note] Note

      NOT the part used in the 3D view is used!

    • Load file: Select the desired part via browse button ....

  • Number of search results

  • Accepted error in finished part

    The error is caused by "missing material" on the unmachined part.

  • Maximum waste in unmachined part

    The maximum waste defines, how much material is allowed to be removed.

  • Resolution

    The resolution controls the search quality. With higher resolution more details are covered, however the search takes more time.

  • Filter for result list:

    A Search for unmachined parts can be combined with a Variables search. Under Section 3.1.2.3.3.1.2.1, “Example - Search for unmachined parts combined with Variables search ” you can find an example on this.

    Detailed information on Variables search is found under Section 3.1.1.6.4.3, “ Variables search ”.

  • Search only in preferred rows

    It is also possible to create a report based on preferred parts. Therefor activate the checkbox. This is according to the activation of the button Preferred rows on/off in the ERP toolbar. Then the report only uses preferred parts.

    [Note] Note

    The on/off state of the button Preferred rows on/off in the ERP toolbar is irrelevant for reports.

  • Unmachined parts to search or Finished parts to search

    At directories to be searched select the checkbox.

3.1.2.3.3.1.1.  Custom variables

With click on the button Edit custom variables the Custom variables dialog box opens.

Custom variables

Custom variables

Here you can define variables, which will be shown at each part in the report in addition.

You can define both ERP variables and variables from the characteristic attribute table.

At first click on Add in order to add a new line.

  • Variable type:

    At first determine the variable type. With double-click on a line under Variable type the list field opens with the following options:

    • ERP

    • Table

  • Variable:

    With double-click on a line under "Variable" a list field with the following input options opens:

    • Options for variable type "ERP":

      The ERP variables from the table are read and displayed in the list field. Select one of the displayed variables or enter yourself a value.

    • Options for variable type "Table":

      The variables of the characteristic attribute table are read and displayed in the list field. Select one of the displayed variables or enter yourself a value.

  • Labeling:

    Enter a label in the input field. It will be displayed in the report later.

  • Unit:

    Optionally you can select a unit in the list field.

    If the variable has no own unit, the selected unit is displayed.

    If the variable has a unit, the value is converted - if needed. (The conversion is only possible for the type "Table".)

    Example:

    The diameter in the table is displayed in "inch". You have selected "mm" in the list field. -> The value is automatically converted from "inch" to "mm".

[Tip] Tip

Already used settings are saved.

Simply select the variable combination, to be displayed in the report, in the list field. If you move the cursor over an entry, all variables with description are shown in a tooltip.

3.1.2.3.3.1.2.  Filter for results:

Via function Filter for results the results can be further restricted. Available is the filter Variables search. You can use the function repeatedly by clicking on Add search function.

[Note] Note

The filter concerns result parts, not the search parts.

The functionality is according to the standard search function:

[Note] Note

It is also possible to create a report based on preferred parts. For this activate the filter Preferred rows on/off in the ERP toolbar before creating the report. Then the report will only use the displayed, filtered parts. Details on this are found under ???.

3.1.2.3.3.1.2.1. Example - Search for unmachined parts combined with Variables search

The following example assumes the mirroring of material groups in an ERP number token. In this case it makes sense to add a Variables search to the Search for unmachined parts.

  1. Select the desired project or directory in the index tree.

  2. Open the respective dialog box via Extras menu -> Search for unmachined parts -> Search unmachined parts for finished part -> Create report... or alternatively via context menu command on the selected project or directory.

    "Search unmachined parts for finished part" dialog box

    "Search unmachined parts for finished part" dialog box

  3. If needed adjust the standard settings. See above.

    In order to add the Variables search click on the blue link Variables search in the section Filter for results.

    Filter for results

    Filter for results

  4. -> The Variables search dialog box opens.

    "Variables search" dialog box

    "Variables search" dialog box

    At the ERP_PDM_NUMBER variable enter the token for the desired material group.

    Now those parts are filtered from the original result list, which ERP number begins with 'BCD'.

    Click on Commit.

  5. -> Now you can see your entry in the Search unmachined parts for finished part dialog box under Filter for results. The filter is already activated .

    Filter set

    Filter set

    In order to display the ERP number in the report, add the variable ERP_PDM_NUMBER under Custom variables.

    Hereto click on the button .

    Set custom variable

    Set custom variable

  6. -> The Custom variables dialog box opens.

    "Custom variables" dialog box

    "Custom variables" dialog box

    Click on Add, select the variable ERP_PDM_NUMBER via list field and confirm wit OK. See above.

  7. -> Now your entry is displayed in the Search unmachined parts for finished part dialog box under Custom variables.

    Custom variable set

    Custom variable set

    Start the search by clicking on OK.

  8. Only parts with the ERP number token 'BCD' are displayed in the report and the ERP number is part of the description.

    Report

    Report

  9. By clicking on Search part... the Search dialog box is opened.

    There you can search for a certain ERP number or for any variable (which is not necessarily displayed in the report).

    Search part...

    Search part...

    By double-clicking on a result part you can jump to the respective place in the report.

  10. In the index tree project/directories where a report is based on, are marked with the icon Available analyses . Mouseover displays a tooltip what the analyses are about.