powered by CADENAS

Manual

Manual

3.1.1.6.4.2.  Full-text search
[Note] Note

In this chapter you can find detailed information concerning Full-text search. This is opened and activated at program start.

You can find detailed information concerning Variables search, Geometric search (3D), Sketch search (2D), Color search and Topology search when you click on the respective link.

You can find information concerning setting options such as "Search for parts and part families" or "Search using Custom selection..., etc. under Search and part selection at a glance. Click on this link.

3.1.1.6.4.2.1.  Full-text search options - Syntax
  • Term query

    A term query is the actual basis for all queries.

    • One term:

      Bolt

      The term "Bolt" can occur anywhere, also as substring. Some examples:

      Through boring for bolts

      Stop bolts

      Bolts with flange

      [Note] Note

      A precise spelling is important. With scrambled letters (blot) or empty spaces (b o l t) you won't get any results.

    • Singular - Plural

      Singular and plural terms lead to the same results.

    • Several terms:

      Each term has to exist anywhere in the project. The sequence is irrelevant.

      Bolt with shank
      Hexagon bolt M10x50

      [Note] Note

      "M10x50" is not yet a variable search in the real sense (on this see under Section 3.1.1.6.4.3, “ Variables search ”), but is contained as text in the table. So empty spaces between the single parameters make a difference. A query with "M 10 x 50" is not successful.

    • Differentiation of character types

      Inserting

      ABC1234DEF

      or

      ABC-1234-DEF

      ABC 1234 DEF

      is also found.[34]

    • Leading zeros in part numbers

      Inserting

      9876

      00009876

      is also found.

  • Term query with NOT operator

    A NOT operator can be used in order to exclude certain terms from the results. Different spelling can be used for this method.

    Bolt NOT reduced shank
    Bolt !reduced shank

    A hit "bolt with shank" for example can be filtered in this way.

    Bolt flush mounted NOT not
    Bolt flush mounted !not

    A hit "bolt not flush mounted" for example can be filtered in this way.

    [Note] Note

    Between exclamation mark (!) and the term to exclude there may not be an empty space.

  • Term query with OR operator

    With the OR operator the search can be expanded to several terms. At least one of the terms has to apply.

    Hexagon bolt OR Head cap bolt

  • Term query with AND Operator (Default!)

    All terms connected by the AND operator have to be part of the result. This kind of query leads to the same result when no operator is used.

    bolt AND shank
    bolt shank

    16.2 21 90
    16.2 AND 21 AND 90

  • Term query with defined sequence (phrase) => "xyz"

    Using quotation marks (") you can determine that the contained terms have to occur in the given sequence.

    Examples:

    • Term without quotation marks:

      Hexagon head bolts with shank

      This search both leads to exact hits and hits such as "Hexagon flange bolts with reduced shank".

    • Term with quotation marks:

      "Hexagon head bolts with shank"

      This search leads only to exact hits such as "Hexagon head bolts with shank", because the terms have to be directly behind one another.

      [Note] Note

      Using the plural form

      "Hexagon head bolts with shank"

      leads to the same hits than using the singular form.

      "Hexagon head bolt with shank"

    A "query with phrase" is automatically generated when a term contains special characters or terms which are composed by characters and numbers.

    AB1-455-PDA => "AB 1 455 PDA"

  • Prefix query (Term query with a wildcard at the end) => *

    Note: The wildcard sign may only occur at the end of a term or a number!

    Note: Adding a wildcard to a term affects the performance (negative)!

    Note: Normally the wildcard search is not needed.

    Bolt*

  • Wildcard query - Terms with a placeholder - ?

    The placeholder '?' can only be used for order numbers. ? is for any single sign instead of the placeholder. Using several placeholders in a row at any position is possible.

    ABC-5?6

  • Wildcard query for a whole directory

    See Section 3.1.1.6.4.2.1.1, “Wildcard query for a whole directory ”.

  • Syntax for table variables

    Full-text search and Variables search can be combined in the input field. With numbers mm supposed.

    Connect the variable name with certain values by using mathematical operators.

    • Variable name with concrete value

      Hexagon bolt L1 = 400

    • In order to search for several variables, use mathematical operators.

      [Note] Note

      Upper or lower case makes no difference for the search term.

      Operators such as AND, NOT, OR have to be upper case.

      Hexagon bolt L > 150 AND D = 20
      Hexagon bolt L = 150 OR D = 20

    • Not only (=) can be used, but all established operators such as (=, <, <=, >, >=).

      Hexagon bolt L >= 120 AND L < 160 AND D = 22

    • Use brackets

      Example 1:

      Hexagon bolts shall be found, either with the characteristic M10x50 or M10x60.

      Search term:

      Hexagon bolt (M10x50 OR M10x60)

      Example 2:

      Bolts with material St37 or St70 shall be found.

      Search term:

      Bolt (st37 OR st70)

3.1.1.6.4.2.1.1. Wildcard query for a whole directory

Performing a wildcard search (*) in the Full-text search input field all projects of the directory set under Search in are outputted.

This can be interesting for a Cloud Map Search or also the export of the search result of a whole directory.

Cloud Map Search:

Example: All handles of the set directory are displayed in the Cloud Map.

Example: All handles of the set directory are displayed in the Cloud Map.

Save search results in a file :

Click on the button .

The respective dialog box opens. Here you can specify the columns to be exported. You can save all search results or only the selected ones.

3.1.1.6.4.2.2. What is searched?

The following data are part of the index. Thus, for those it can be searched in all languages:

  • Project

    • Path

    • NT

    • NN

    • Date

    • Catalog name

  • Table (+ERP)

    • NB

    • Fixed numerical values

    • Fixed textual values

    • Order number (defined by CNSORDERNO)

    • Value range variables with fixed values (no value range)

  • Classifications

    • EClass IDs or class description

    • Class attributes

Examples:

  • The Project path is displayed on the tabbed page Search results, on project level, in the column Summary.

    When searching in another language than the set one (in the next figure exemplarily "schraube") you can see in the popup window under Hits (Treffer) where the hit is based on [NB (standard name), path and description].

  • In the following a search with "head cap bolt ISO" is conducted.

    The respective terms are marked on the tabbed page Search results:

    On project level: In Standard number (NN), Standard text (NT) and Project path

    On line level: In Standard number (NN), Standard text (NT) and Standard name (NB)

  • Hits based on table values are marked in yellow on the tabbed page Search results as well. In the following example a search for "hexagon bolt D=10 L=50" has been performed.

3.1.1.6.4.2.3.  Automatic phrase completions

While typing into the field Full-text search a list field is automatically opened and proposals are offered which can complete the search term.

Example: When "cd" is entered several cylinder designations such as "CDN" or "CDVI" are offered for example.

Example: When "cd" is entered several cylinder designations such as "CDN" or "CDVI" are offered for example.

With the tab key you can overtake a selected term from the list, with the return key you can overtake a selected term and a search is directly executed.

The displayed proposals also depend on the selection under Search in.

[Note] Note

The display of proposals does not automatically mean that a combination of terms really leads to hits, but instead that each single term exists.

Example: "Hexagon head bolt with nipple" will not lead to any hits.

Example: "Hexagon head bolt with nipple" will not lead to any hits.

3.1.1.6.4.2.4.  Full-text search supplemented with synonyms

If Search for synonym is activated, then the synonym database is automatically searched based on the inserted keyword. A tooltip appears with supplemental terms.

[Note] Note
  • The evaluation of found synonyms is the same as for the inserted search term.

  • In order to find the synonyms in the synonym database, the exact same spelling is crucial. With scrambled letters (blot) or empty spaces (b o l t), the synonyms based on bolt cannot be found.

The synonym database can be enhanced be administration anytime. On this see under Section 1.1.8, “ PARTsynonym ” in PARTsolutions / PARTcommunity4Enterprise - Administration Manual.

3.1.1.6.4.2.5.  Full-text search in link database using ERP integration

When using the Full-text search, projects and link database are always searched together. Even if several search terms are used, it makes no difference whether hits score in the project file or in a LinkDB column.

On this see under Section 3.1.2.7.2, “ Enhanced search possibilities with ERP integration ”.

3.1.1.6.4.2.6.  Full-text search example

The following example shows a complete search with setting search options, result list and starting the part view.

  1. Limit the search at "Current selection (ISO)" and leave the setting "Search for parts and part families".

  2. Enter the following into the input field:

    hexagon bolt L >= 120 AND L < 160 AND D = 20

    [Tip] Tip

    When you open the list field under Full-text search, then you see preceding inputs, which you can simply select with a single-click. So you can possibly save complicated entries.

    Should you have removed the full-text search via click on from the list of search methods, then simply click on the link .

    -> The Full-text search dialog box opens and you can perform an entry anew.

  3. Click on Start search.

    -> The search results are listed on the Search results tabbed page. When you click on the plus sign , then you can see the single parts of the part family below. The following figure shows 4 lines, which exactly meet the search criteria (D equals 20 and L is between 120 and 150).

  4. Click on the icon Open.

    -> The view switches to the Part view.

  5. Select the Table tabbed page.

    Part view in"Table" mode

    Part view in"Table" mode

    Top left at the icon Search filter on/off you can recognize, that the characteristics have been filtered. When you want to see all characteristics, click on the icon.

    Select the List tabbed page.

    Part view in "List" mode

    Part view in "List" mode

    Also here you can recognize at the icon Search filter on/off , that the characteristics have been filtered. When you want to see all characteristics, click on the icon.



[34] Other special characters are handled in the same way.