powered by CADENAS

Manual

Manual

3.1.7.1.10. Show topology variables in table

Topological variables can be displayed beside the standard table information. With the checkbox Topology variables you can activate / deactivate the display if needed. Especially at own part catalogs characteristic values are not necessarily in the characteristic attribute table. In this case the display makes sense in particular.[73]

Topology variables in table

Topology variables in table

Precondition is that the desired topological columns have been chosen in the settings dialog. On this, call the settings dialog by clicking on Table settings and activate the checkbox under Show topological values. There, you can activate/deactivate the desired topology types.

Settings: Show topological values

Settings: Show topological values



[73] Missing topological values are not generated on the fly, but available values are displayed. In standard catalogs, mostly this is a certain percentage, in own part catalogs normally topological values are available for all table lines.

In the docking window Topology information topological values are generally displayed (see Section 3.1.7.9, “Docking window "Topology information "”).