powered by CADENAS

Manual

Manual

3.1.10.1.2.1.  Render mode

In the list field under Render mode the display under the derivation may be changed:

Choose one of the following options in the list field:

  • Line view:

    Line view

    Line view

  • Lines + shaded view:

    Lines + shaded view

    Lines + shaded view

    Combination of line display and shaded display

    Advantage: Optically more attractive than line display

  • Shaded View:

    Shaded view

    Shaded view

    Here a gridded image is displayed, into a 2-D derivation. The derivation is only created if an export to the CAD system follows.

    Advantages:

    • Optically more attractive than line display

    • Very rapid display, also with complex parts

    [Note] Note

    This render mode is also used for creating 3-D datasheets [93] See under Section 3.1.9.4.4, “Export PDF datasheet ”. The speed factor comes into play here.



[93] For PARTcommunity as well