powered by CADENAS

Manual

Manual

3.1.9.2.9. "Export options" tabbed page - DXF 2D (binary)

[Note] Note
  • When exporting into the dxf file, the information of the tabbed page Layers is stored in the file.

    Example: "Thick lines" are mapped to layer "AM_0" and are stored in the dxf file in yellow.

    Example: "Thick lines" are mapped to layer "AM_0" and are stored in the dxf file in yellow.

    If the file is imported into an existing drawing, then CAD settings have priority.

    Example: Mechanical-Layer-Manager: AM_0 = white. The inserted part is depicted with white "Thick lines".

    Example: Mechanical-Layer-Manager: AM_0 = white. The inserted part is depicted with white "Thick lines".

    If the file is opened apart, then the depiction will be with the layer color specified in the dxf file.

  • Layers not existing in the CAD are created according to the defaults.

  • If you want to override CAD layer information, then use the tabbed page Export options.

    Example: In this case the "Thick lines" are depicted in blue.

    Example: In this case the "Thick lines" are depicted in blue.

  • Tabbed page Layers

    Tabbed page "Layers"

    Tabbed page "Layers"

    • Open directory after export(once)

    • Destination file

    • Version

  • Tabbed page Export options

    Tabbed page "Export options" - DXF 2D (binary)

    Tabbed page "Export options" - DXF 2D (binary)

    • Insertion position: The insertion position in the CAD system can already be set in PARTsolutions - assuming your CAD system supports this function. Enter the X and Y coordinates..

    • No Attributes : ...prevents certain attributes (for example texts from PARTproject) from being transferred to the CAD system during export.

    • Line and color settings:

      Aside from the possibility of directly assigning lines and colors, the color and line settings may also be made dependent on the layer setting in the CAD system. For this, select the option "by layer".

    • Open directory after export(once)

    • Destination file

    • Version