powered by CADENAS

Manual

Manual

3.1.12.4.3.  Table

In the table view, you can see the individual variable values.

[Note] Note

The table shows each selected element in the Connection dialog area. To change the single part table, click on the marked connection components.

Every change in the dialog window Connection is immediately shown in the table. The vertical view shows pinning of values with the help of the checkmark immediately.

In the "Connection" dialog area "Nominal" and "Length" are pinned. The list view adapts this information.

In the "Connection" dialog area "Nominal" and "Length" are pinned. The list view adapts this information.

In addition to the selection in the Connection dialog area, value ranges can still be set in the table (both in the list view and table view). When saving connections these are also saved.

Define value ranges

Define value ranges

The view type in the table can be changed via the Table and Vertical tabs. A detailed description can be found under Section 3.1.7, “ Part view ”.