powered by CADENAS

Manual

Manual

2.6.4.4.1. Determine variables in List view

When opening the tabbed page View, all variables are displayed in a List view by default.

The list view is subdivided with the following columns:

  • Name of variable with Variable description

  • Variable value

    There are different possibilities:

    • Fixed value

    • Value selection of a standard variable

    • Value selection of a value range variable

    Via input fields, list fields, sliders, etc. the value can be changed (if basically possible).

  • Symbol to describe the current status of respective variable.

    Especially interesting is, whether a part is already uniquely specified and/or if there are more options available.

Details on this can be found Section 3.1.7.2, “Determine characteristic in "Vertical" view ”.