powered by CADENAS

Manual

Manual

3.1.7.1.11.5. Example: Using filters

  1. Full-text search for Hexagon bolt M10

    The table only shows parts with nominal diameter 10.

    The table only shows parts with nominal diameter 10.

  2. In addition, in the column header, setting a filter on length 40.

    Now both filter icons are displayed (limitation by search + table filter).

    The table only shows parts with nominal diameter 10 and nominal length 40.

    The table only shows parts with nominal diameter 10 and nominal length 40.

  3. Clicking search filter (= deactivation).

    -> Now all rows with L=40 are displayed. Characteristic M8x40 has an ERP number.

    Table shows all rows with nominal length 40.

    Table shows all rows with nominal length 40.

  4. Alternative approach via preferred rows filter

    Delete all filters set before, activate preferred rows filter and perform a new search.

    Now you will find all parts with existing ERP number.[75]

    If the use of a M8 bolt is also possible, this is advantageous because the part already exists in the ERP system and so is released.



[75] Please also regard the search range set under Search in.