powered by CADENAS

Manual

Manual

3.1.9.5.1.1. Export in native format

Via the Native menu icon, you can export deposited native parts from PARTsolutions into any directory.

[Note] Note

The Native command is only active if you loaded a native part.

Export in native format

Export in native format

Native parts can, among other things, be deposited in the following way in the PARTdataManager directory structure:

  • With interface:

    From the interface menu within the CAD system via User library -> Insert. See Section 2.6.15, “ User library ”.

  • Without interface

    Via PARTadmin -> Category Index administration -> Import. See Import von Geometrie-Dateien.

On the Export in native format dialog page, make the following settings:

Export in native format

Export in native format

  • Output directory for native parts:

    Via Browse ... set the output directory:

  • CAD system: Enter a description in the input area.

  • Destination file: Is already set, do not change.