powered by CADENAS

Manual

Manual

4.8. How can I generate CAD models?

In order to generate CAD models please click on the button CAD or Generate CAD.

By default, you can find the button above the preview.

"CAD" button (example B2B portal)

"CAD" button (example B2B portal)

Depending on portal it also may be placed above the table.

"Generate CAD" button (example Supplier portal)

"Generate CAD" button (example Supplier portal)

[Note] Note

Before generation the required CAD formats and methods of providing have to be determined. For this click on Formats. More details on this can be found under Section 4.7, “How can I select CAD formats?”.

If no formats are yet specified, the Format selection area is automatically opened.

Directly after clicking the button the generation is started. Generated models are displayed in the right panel. More details on this can be found under Section 4.9, “How can I import the selected CAD model into the CAD system?”.

Display of generated models in the download area for different methods of providing (example B2B portal)

Display of generated models in the download area for different methods of providing (example B2B portal)