powered by CADENAS

Manual

Manual

3.1.11.7. Hiding columns

Specific settings in PARTsolutions are saved on the local desktop computer and can be changed by the user himself; e.g. a list of suppressed columns.

Via Extras --> Settings menu item, the respective dialog is opened. Under Table menu item, in the input field Columns to hide, enter the names of columns (separated by comma) that should not be shown.

The following figure shows the result of the options change:

The ACTIVE_STATE column is hidden now.

Normally this setting concerns ERP columns, which are not needed by a certain user.Hiding columns by administration is also possible, of course. See Anzuzeigende Spalten - plinkgroups.cfg -> Block [Role_name] -> Key "VARSUSED / VARSHIDDEN".

Normally this setting concerns ERP columns, which are not needed by a certain user.[102]



[102] Hiding columns by administration is also possible, of course. See Section 4.12.2.1.6, “ Columns to be displayed - plinkgroups.cfg -> Block [Role_name] -> Key "VARSUSED / VARSHIDDEN" ” in PARTsolutions / PARTcommunity4Enterprise - Administration Manual.