powered by CADENAS

Manual

Manual

2.6.12.  Topo Search

[Note] Note

The Topo Search is hidden by default. In order to activate, in PARTadmin -> Configuration files -> ifacecommon.cfg, filter for "406" and activate all displayed keys. After restart of PARTdataManager and CAD system the function Topo Search will be displayed in the PARTsolutions toolbar. Information on UI design can be found under Section 2.2.1.6, “Configuring PARTsolutions interface menu and toolbar ” in PARTsolutions / PARTcommunity4Enterprise - Administration Manual.

[Note] Note

Currently the Topo Search is only available for cone and cylinder faces.

  1. Click on Topo Search and then on a cone or cylinder face.

    -> If Seamless has not been started yet, this will happen now.

    -> Furthermore the dialog box Topology search is opened. The adequate method (below in exemplary figure this is "Cone") is already opened and values detected from the selected face are already entered in the input fields.

    Topo Search

    Topo Search

  2. If needed, adjust tolerance and start searching by clicking Apply -> Start search or Commit and Search at once.