powered by CADENAS

Manual

Manual

3.1.6.4.3. Search for Order number or type code

Use this search method in order to search for Order number or type code. Hereto, beside the input field of full-text search, click on the right button .

Fixed order numbers can also be found via Full-text search. If however an Order number or Type name is combined from values of value range variables, there is a huge number of possible combinations, which cannot be tracked by the standard index, so that the Full-text search won't lead to results.

Example project with many value range variables, which build up the part number

Example project with many value range variables, which build up the part number

With this search method you will find order numbers and/or type code in any case (provided the catalog is prepared accordingly).

[Note] Note
  • Fixed order numbers can be found with Full-text search further on.

  • Please pay attention to upper and lower case.

  • With existing ERP integration the following applies: At rows with existing ERP number ALL variable values are indexed in the standard index and so can be found with Full-text search.

  • The search method Order number or type code cannot be combined with all other searches, so they are disabled (grayed out).

  • The button can be hidden via config setting. On this see Section 1.7.5.19.4.2, “ Key "TOP_SHOW_REVERSE_SEARCH"” in PARTsolutions / PARTcommunity4Enterprise - Administration Manual.