powered by CADENAS

Manual

Manual

2.5.5.2.4.  Insert model - Pattern recognition

In the following, the process is described if patterns are found:

Initial situation: After transferring the placement part to Creo via Transfer to CAD the view returns to Creo and the placement dialog is opened.

The PARTsolutions placement dialog box opens

The PARTsolutions placement dialog box opens

  1. Click on the button In hole .

  2. Select one or several holes.

    One hole selected

    One hole selected

  3. Click on the button Place multiple (dialog stays open when process finished) or Place once .

    -> The dialog box Place part is opened querying "Muster mit Instanzen füllen?"

    Now you have two options:

    • Fill pattern with instances

    • Create instances only at selected locations

    Click on the button Choose.

    -> The desired instances will be placed.

    Instances only at selected positions

    Instances only at selected positions

    All instances filled

    All instances filled

  4. If PARTsolutions placement dialog is opened, close it by clicking Close dialog .