powered by CADENAS

Manual

Manual

3.1.6.7.1.5. "Partition Map" display mode

In the mode Partition Map the results are partitioned in rectangles.

At first the main level is displayed, always four cluster with four representatives each. So you have 16 options. When clicking on a cluster you see further images and automatically zoom in, step by step down to the lowest level with parts. In each cluster the number of contained results is displayed in the top right corner.

Example 1:

In some clusters, it has been zoomed in and then out in order to search at another place.

In some clusters, it has been zoomed in and then out in order to search at another place.

Example 2:

On the lowest level, in the "Partition Map" as well, you can call up the 3D view via mouseover or open the part in the "Part view" via context menu command as usual.

On the lowest level, in the "Partition Map" as well, you can call up the 3D view via mouseover or open the part in the "Part view" via context menu command as usual.

[Note] Note

An inactive (grayed out) command shows that the special index has not yet been created. See Section 1.3.8.6.2, “Context menu commands in detail ” in PARTsolutions / PARTcommunity4Enterprise - Administration Manual -> Geometrical search index -> Create partition map.