powered by CADENAS

Manual

Manual

2.2. Integrating the PARTsolutions interface

The integration of the PARTsolutions interface occurs automatically if your CAD interface was selected in the respective section of the PARTsolutions installation.

The interface is then stored under ... $CADENAS\iface\"cadname".

It is possible that CAD specific settings must still be made in order to make the PARTsolutions menu visible.

The configuration files can be found under $CADENAS_SETUP/if"cad_shortcut".cfg.[1]

Under PARTadmin -> category CAD integration you can check, if interfaces are installed and if they are in activated or deactivated state, furthermore manually change activation/deactivation. See Section 1.3.3, “ CAD integration ” in PARTsolutions / PARTcommunity4Enterprise - Administration Manual.



[1] More detailed information can be found under Chapter 2, PARTsolutions - CAD Integration - Administration in PARTsolutions / PARTcommunity4Enterprise - Administration Manual.