powered by CADENAS

Manual

Manual

5.12. Error in LINKTABLE

LinkDB has newer entries than loaded version.

PARTdataManager

The link database does not match the catalog version that was loaded.

The export is now blocked. Also the visible material numbers are possible displayed incorrect.

Possible reasons

- A catalog update was not synchronized to the current location (remote location installations only).

- You loaded an old version of the project.

- There is a serious error in the Database.

If this message is still visible in 24 hours please contact the administrator.

OK

Information about fixing this error can be found under Section 4.16.3.3.1, “Update without connection to the LinkDB ” in PARTsolutions / PARTcommunity4Enterprise - Administration Manual.