powered by CADENAS

Manual

Manual

2.3.1.3.3. Block [BomNormalAttributes] - Define BOM list attributes

In the block BomNormalAttributes you determine which PARTsolutions attributes are to be exported to the BOM list.

Optionally you may also change the field entries or insert text or variables into empty ones.

Per Default only the attributes "Description", "Standard" and "Material" are displayed in the BOM list (BOM list table) in AutoCAD.

Example 1: Standard attributes in the BOM list

Example 1: Standard attributes in the BOM list

If you add columns to the BOM list window, you can see which other attributes were exported from PARTsolutions in the window Select columns (compare to fig. ???). As soon as you have inserted the columns, these are made visible with the PARTsolutions export value.

BOM list enhanced with the attributes "Name" and "Supplier"

BOM list enhanced with the attributes "Name" and "Supplier"

BOM list table with the desired columns inserted into the drawing:

Example 2: BOM list table with extra attributesBOM list table, enhanceAutoCAD

Example 2: BOM list table with extra attributes