Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
"Named User" licenses represent "centrally managable" nodelocked licenses. They are bound to the FLM server, just like normal "floating" licenses. Other than floating licenses, they are not released after a module terminates. Each instance of a named user license is bound to a user account permanently. The assignment is done automatically when a client requests a license for the specific product. Existing assignments can be changed here, after a minimum hold time has passed.
The minimum hold time is 24 hours at the first change, 30 days at the second.
On the tabbed page Named User, in the column Product, all products are listed.[36] The columns Assigned count, remaining free, Total and Latest change contain additional information for each license product.
For each license product there are two possible base settings:
The checkbox in the column Assign automatically? is activated. This is the default setting.
Once a client requests the license in the selection dialog box of the module, it is dynamically assigned to it from the pool of available licenses.
All users which ever accessed the FLM server are listed under Known users. All users to whom a license has been assigned are displayed under Assigned users.
The checkbox in the column Assign automatically? is deactivated.
In this case the desired user has to be manually assigned for a certain license product by administration.
All users which ever accessed the FLM server are listed under Known users. If the desired user is not listed yet, add him via input field and click on the button.
In the dialog area Known users select the desired user.
Should the list be very long then you can filter by any text string of the user name.
In the dialog area Assigned users, insert the user by clicking on or . Then in the column Assignment type "manual" is displayed.
Once everything is set up correctly, click on .
Via you can remove a user from the dialog area Assigned users again, which has been added by clicking on ; however only as long as you did not save yet.
Independent of the settings under Assign automatically? another user can be assigned after expiry of the minimal dwell time/wait lock via .