Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
Note | |
---|---|
As of V10 catalog modeling does not use it anymore. Markup of parts to be avoided now happens in the characteristic attribute table by a special standard variable CNSAVOID. On this see Section 9.8.9.2, “Mark parts to be avoided ” in eCATALOGsolutions Manual. |
In the DIN, EN and ISO datasheets (as well as other country standards) certain sizes are sometimes considered to be avoided.
Via configuration (set for standard parts by CADENAS and may be changed administratively by customer) these sizes may be marked or hidden.
Tip | |
---|---|
The following markups of parts complement each other:
|
The configuration happens in PARTadmin as described below:
Block [COMMON] contains the following keys:
A complete definition is contained in each block pair.
First the block, which defines the rule, then the block which is referred by the desired project.
Block [Rule name] contains the following keys:
[STD-SCREWS-2] RULE1=D.EQ.3.9 [norm/din/schrauben/blechschrauben/din_6928_c.prj] RULE1=STD-SCREWS-2