powered by CADENAS

Manual

Manual

4.17.3.  Pinning Dimension attribute OnOff / plinkcommon.cfg -> Block [PARTdataManager] -> Key "LockDimRange"

[PARTdataManager]
LockDimRange=0 (value 0 or 1)

With LockDimRange, the decision is made whether the Dimension attribute for example, the length of a semi-finished part) is to be pinned or not.

Semi finished product - Dimensioning attribute not pinned

Semi finished product - Dimensioning attribute not pinned

  1. LockDimRange = 0

    By double-clicking on the yellow field, an input window opens in which you can set the variable value (for example the length 'L').

    The part is exported with the set value.

    After reloading the part, the value is set back to the original value of '100'.

  2. LockDimRange = 1

    The pinned (in other words unchangeable) value is no longer displayed in yellow, but with a white background.

    Pinning occurs through the assignment of an ERP number.