Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
2.3.7.4.
Attribute mapping in Solid
Edge
2.3.7.4.6. Fill more
fields in Solid Edge with PARTsolutions attributes
|
|
---|---|
Prev | Next |
You want, for example to fill the additional field Manager in the file properties on the Info tabbed page in Solid Edge.
From the table get the correct field name (see Section 2.3.7.4.6.1, “ Field names in Solid Edge”) and remember in which block it shows up (Manager shows up under DocumentSummaryInformation)
Under PARTadmin -> Category -> Configuration files -> $CADENAS_SETUP -> ifsolidedge.cfg open the block DocumentSummaryInformation.
Insert a key. In this example "Manager".
Enter a value. In the figure above
?"Me"
This simple syntax can be used for simple text output
The key name in PARTsolutions corresponds to the field description in Solid Edge. The key value is the output text in Solid Edge.
-> The Manager field is now completed.