powered by CADENAS

Manual

Manual

1.7.5.19.3.  Block [EOLService] - Show/hide lines to be avoided

In the DIN, EN and ISO datasheets (as well as other country standards) certain sizes are sometimes considered to be avoided. If the option is activated, lines to be avoided are marked in the PARTdataManager Part view.

In order to show/hide parts uses the button Show/hide lines to be avoided.

Settings on this are carried out in the block [EOLService]:

  • LinkdbVariants: Show/hide LinkDB variants in the table

    • true: LinkDB variants are not basically hidden and the visibility can be controlled via .[23]

    • false: LinkDB variants are principally hidden.

  • ShowLines: Show/hide the "to avoid" lines in the table

    • true: Lines marked with "to avoid"[24] are not basically hidden and the visibility can be controlled via .

    • false: Lines marked with "to avoid" are principally hidden.

  • ShowButton: Activation/Deactivation of the button

    [Note] Note

    Hiding the button is controlled via menuvisibility_PARTdataManager.cfg.

Display position in UI:

  • ToolBar: The button is displayed on the here stated toolbar. Default is Standard toolbar.

  • ButtonAfter: The button is displayed before the here stated button. Default is "din962".



[23] With existing ERP integration LinkDB variants can be created via . On this see Section 4.7, “ERP toolbar and menu ”.

[24] The markup happens on the side of catalog manufacturer. On this see Section 9.8.9.2, “Mark parts to be avoided ” in eCATALOGsolutions Manual.