Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
Central point of the user-role concept is the rights administration.
The rights and thus the user interface can be specifically designed so that part selection and new creation of parts can be controlled.
The creation of the user-role concept is performed in the module PARTadmin.
The corresponding dialogs are found under category ERP environment with the sub-categories User and Roles.
In the following the most important substeps for the creation of the user-role concept are described.
General notes on the concept can be found under Section 4.1.5, “ User-role concept”.
A detailed description on the creation of the single roles can be found under Section 4.12.2, “ Create and configure roles ”.
Create Database user in the database:
Create users via SQL scripting with the database: See Section 4.2.4, “Create database scheme and users for ERP (exemplified by MSSQL)”.
Create users via PARTadmin -> category ERP environment -> subcategory User im Dialogbereich Database user
Here you can directly access the database, if the login happens with admin password.
Create
users in PARTsolutions, in the
configuration file plinkusers.cfg
.
On the side of PARTsolutions users are stated under category ERP environment -> sub-category User -> dialog area User (in order to set up the role assignment afterwards).
All created
users are saved in the configuration file $CADENAS_SETUP/plinkusers.cfg
.
Each user is represented by its own block.
[ecat] GROUPS="ECAT1","ECAT2" GROUPORDER="ECAT1","ECAT2","ECAT3","ECAT4","ECAT5","ECAT6","LOC1","LOC2","LOC3" [location] GROUPS="LOC1","LOC2" GROUPORDER="ECAT1","ECAT2","ECAT3","ECAT4","ECAT5","ECAT6","LOC1","LOC2","LOC3"
Roles (groups) are managed under ERP environment -> Roles. Any rule, very complex ones as well, can be specified here.
Details on this can be found under Section 4.12.2, “ Create and configure roles ”.
The assignment of users and roles happens under category ERP environment -> sub-category User -> User-Role assignment