Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
This module enables the integration of company-owned META data into the PARTsolutions software.
You can connect attributes from the META data, such as for example internal article numbers, price, material, part status, etc., with the installed standard attributes of the PARTsolutions supplier catalogs.
The module covers the following functionalities:
PARTlinkManager ― Administration tool for all ERP relevant data[55]
Display and changes of datasets in the LinkDB (in the LinkDB you can find all information about the connection concerning part allocation to ERP master data)
Adjustment of visual display of data in the PARTsolutions environment (example: different coloring for individual rows according to condition)
PARTadmin - Configuration tool for PARTsolutions and administration tool for roles and users.
PARTsolutions Toolbar [56]
Database scripts - Predefined scripts for creating the LinkDB, which can be used with PARTsolutions.
Currently available for Oracle, MS SQL, DB/2 and SAP DB[57]
ERPsolutions/gateway JDBC - Gateway for access to databases via Java DataBase Connectivity
JDBC is a Java based version of the database access (to LinkDB).
JDBC works cross-platforms, available for all Unix platforms.
The package does not include the JDBC drivers for the corresponding databases. They have to be provided by the customer.
As far as free drivers are available, JDBC-drivers (free of cost), which are available under the LGPL-license are additionally enclosed in the package, they are not supported by CADENAS and no guaranteed content of the scope of delivery.
For installation and implementation to ERP environments an individually arranged consulting package is urgently recommended.
PARTsolutions/development partwarehouse ident mapping&synchronize
Includes command line tool to transfer attributes from the ERP system (e.g.) for ERP/PLM integration) assimilation of company specific part data (part numbers and attributes) from one database and transfer to PARTsolutions tables
Includes PARTdataCenter GUI for comparison of ident numbers: Interface for assigning ERP numbers semi-automatically
For data flow of the ERP-System towards the PARTsolutions database, there are different implementation possibilities (so called linking methods e.g. cyclically replication, trigger replication, …), depending on the environment and the customer’s needs. For a „real“ online linking to the ERP system (which means generating new part numbers directly from PARTsolutions), additionally to the ERP-module a ERPsolutions/gateway is necessary (e.g. ERPsolutions/gateway SAP MM or an individually programmed gateway).
[55] Detailed information can be found under ERP-Umgebung konfigurieren and Section 4.13, “Manual data administration ”.
[56] Detailed information on this can be found under PARTdataManager – ERP/PDM Erweiterungen.
[57] The
scripts can be found on the installation medium under
/tools/databases
.
Detailed information can be found under Section 4.2.4.1, “Installations script ”.