powered by CADENAS

Manual

Manual

4.17.8.2.2. Assembly with ERP numbers

Now assign an ERP number for one of the rows of the assembly (again via Add dataset to link database ).

[Note] Note

As soon as an ERP/PDM number was assigned to the main table, a stencil is created and deposited in the database. This is then loaded again by selecting the same one so that the ERP/PDM numbers of the sub-parts can also be restored.

PARTlinkManager - stencil

PARTlinkManager - stencil

The status light is now set to "green", analogously to that of Export restriction.

Select this row.

Select "Assembly" in the "Assembly" window.

Assembly with ERP number

Assembly with ERP number

[Note] Note

In the"Assembly"window th fields under "ERP_PDM_NUMBER" are grayed out!

As soon as an ERP number has been assigned to an assembly you may no longer be able to change single parts!

Select "hinge wing" in the "Assembly" window. --> In the main window you now see the part built into the assembly.

Part List - Select single part

Part List - Select single part