powered by CADENAS

Manual

Manual

4.25.7.6. Import project into database

You can import individual projects and entire directories into the database. You have the following commands available.

  • Import this project in database (at project level)

  • Import only projects from this folder (at directory level)

  • Import from all sub-folders (at directory level)

[Caution] Caution

When importing an entire folder it is possible to import more than 1000 datasets! Therefore be especially careful when using the 3rd command.

The project is imported into the database complete with all rows. All datasets under Active status contain the entry "Locked", and under Requested status there is no entry.