Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
The configuration
file ifacecommon.cfg
contains general CAD encompassing settings.
If changes should be necessary please conduct them under PARTadmin -> Category ->PARTsolutions -> Configuration files -> $CADENAS_SETUP -> ifacecommon.cfg.
The following table gives an overview on the individual blocks.
Block | Key | Description |
Macros |
Macros contain a sequence of instructions or declarations under a certain name, in order to execute these with one simple command (instead of the single commands). |
|
Categories |
Explanations on categories can be found under Section 2.2.1.1, “ What are categories?”. is2d The expression is valid, if the document is a 2D element. |
|
Categories | isCatalog | |
Categories | isUser | |
Categories | isHost | |
Categories | isProject | |
Categories | isProjectFile | |
Categories | is2d | |
Categories | is3d | |
Categories | isNat | |
Categories | is3dAsm | |
Categories | is3dPart | |
Categories | isInchDoc | |
Categories | isMMDoc | |
Categories | isNotRootDoc | |
Categories | isRootDoc | |
Categories | isSubAsm | |
Categories | isSubPart | |
Categories | isPartConnectionAsm | |
Categories | isPartConnectionPart | |
Categories | isPartConnectionExport | |
Categories | isNegativePart | |
Categories | NotWindows | |
Categories | Windows | |
Interface | Currently only contains deactivated keys | |
CreationOptions | ||
CreationOptions | NoSection |
For connection elements such as bolts, nuts, rings, etc. cutting in the 2D view can be excluded. |
PDM |
Default callbacks. You can customize the callbacks here (or overwrite them in the specific interface configuration). |
|
UI |
Design of PARTsolutions interface menu and toolbar Details on this can be found under Section 2.2.1.6, “Configuring PARTsolutions interface menu and toolbar ”. |
|
Placement |
Also see Section 2.2.8.4, “Block [Placement]”. |
|
NativeCheckin3 | Also see Section 2.2.8.5, “Block [NativeCheckin]”. | |
ClassMapping |
Mappings 1 to 7 create the mapping for the material First choice is the "MAT_NAME" column in the characteristic attribute table (used with ERP integration). Second choice is the "virtual" column "CNSMAT" (without ERP integration). Also see Section 2.2.8.6, “ Block [ClassMapping]” and Section 2.2.5, “Material mapping ”. |
|
CustomExec | ||
LOD |
This settings concerns the level of detail for the export.
|
|
CalcName | ||
CADEXTENSIONPRT |
The CAD extensions should be administrated here (used e.g. by plm interfaces) |
|
CADEXTENSIONASM |
The CAD extensions should be administrated here (used e.g. by plm interfaces) |
|
TranslateRessourceText | ||
GeoSearch | Currently not in use | |
PROXIES | ||
iface.<cadname> | Blocks concerning the single interfaces |
Note | |
---|---|
You can receive more information on single blocks and keys, if you click them under PARTadmin -> Category ->PARTsolutions -> Configuration files -> $CADENAS_SETUP -> ifacecommon.cfg.
|