powered by CADENAS

Manual

Manual

4.25.7.7.1. Change standard descriptions according to project

Assign the standard description (NB) for individual projects differently from the standard defined NB if desired.

Complication naming rules can only be solved via an external vbs script.

In the PARTlinkManager, in the directory tree at project level, you have the command Edit project table available to you.

The Edit table opens after activation.

Edit project table

Edit project table

Select the row standard name in the pull-down menu of the VKEY.

Under VVALUE you can now define any standard name. For example: my_NB_$D.

Address variables with $Variable. Take possible variables from

Section 6.1.3, “Constants ”. All ERP variables are also possible.

For SHORTNB or LINA continue analogously.