Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
Common PARTsolutions configuration files
Settings for the 2D view in PARTdataManager
Details on this can be found under Section 4.11.3, “ 2D derivation: Create your own Combination views ” in eCATALOGsolutions Manual.
DIN 962 controls how screws and nuts can be adjusted for certain use cases through additional forms and information.
material.cfg (without ERP integration)
Client settings of the PARTapplication Server. See Section 4.5.6.1, “ AppServer: Client configuration”.
Server settings of the PARTapplication Server. See Section 4.5.6.2, “ PARTapplicationServer: Server configuration”.
Settings for all PARTsolutions modules, especially PARTdataManager GUI settings
Configuration files for CAD interfaces
CAD specific
configuration files if<cadname>.cfg
and
ifacecommon.cfg
.
See Chapter 2,
PARTsolutions - CAD Integration - Administration.
Configuration files for ERP integration
Common ERP settings. In the user interface you can find most of the setting options under PARTlinkManager -> Extras menu -> Configure ERP environment.
To see the features embedded into the context of Strategic Parts Management please see Chapter 4, Strategic Parts Management .
Contains groups (syn. roles) of the single users. In the user interface you can find most of the setting options in the Category tree under Roles.
To see the features embedded into the context of Strategic Parts Management please see Chapter 4, Strategic Parts Management .
Contains the created users. In the user interface you can find the corresponding settings in the Category tree under User.
To see the features embedded into the context of Strategic Parts Management please see Chapter 4, Strategic Parts Management .
The configuration file erpcustom.cfg
is used in order
to further customize ERP processing. For example, one important setting
is for the user dialog when adding datasets to the LinkDB.
material_assign.cfg (with ERP integration)
Material specifications for export
See Section 4.10.1, “ material_assign.cfg (with ERP integration) ”.
Used to establish the nightly transfer of third party system information to PARTsolutions.
Contains settings for Export tables (PARTlinkManager -> Extras menu -> Configure ERP environment -> Export tables tabbed page).
Contains basic settings on Update manager, which normally don't have to be changed. For details on Update manager please see Section 4.16.3, “ Catalog update with ERP integration - Fix mapping problems with the Update manager ”.
For the database connection data, i.e. Server, Database, in particular the driver class and the URL for the jdbc driver to establish a connection to the database.