Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
$CADENAS_SETUP/ erpcustom.cfg
:
This configuration file is used in order to customize ERP processing.
The file is subdivided in a couple of blocks:
USERDIALOG, VARS, LOAD, BEFTBLLOAD, AFTTBLLOAD, MAIL, ADDTODB
Entries can be made per group (role). Thereby the behavior of PARTsolutions can be adjusted on role level.
For details see Section 4.11, “Timestamp number on/off”.
When using the SAP MM Schnittstelle also see Customizing der PARTsolutions-ERP-Schnittstelle.
The block VARS contains common keys.
The following entries can be made per group (role). Thereby the behavior of PARTsolutions can be adjusted role-specific.
[VARS(Rolle1)]
Key value is the variable name of the database column. In the user interface, you can set it in PARTlinkManager under Extras menu-> Configure ERP environment.
If you enter a database field here the ERP number is copied into this field (for multiple locations only).
0: The ERP number entered by the user or the number returned by the ERP system is inserted in the link database.
1: A so called timestamp number is generated and inserted into the link database. This setting only makes sense in special cases (e.g. at multiple location systems).
ERPADD=$CADENAS_SETUP/erpadd.cfg
Contains
the path to the configuration file erpadd.cfg
.
The block name contains the path to the PARTsolutions project file (part family), the key name is the identifier for the ERP-System, key value is fixed or a variable name of the PARTsolutions table. A variable name starts with a $ character and ends with . (point).
[norm/din_en_iso/schrauben/zylinderschrauben/din_912.prj] NAME=Screw FIELD1=$D.
The given entry is searched in the respective PARTsolutions project file and exported to the ERP system.
|
Address of the e-mail sender when requesting a new ERP number via e-mail.
Name of the e-mail server for requesting a new ERP number via e-mail.
State of the new created part.
Possible values are 0 (locked), 1 (released) and 2 (expired).
See Section 4.21.2, “ Default value for new "ACATIVE_STATE" values - erpcustom.cfg -> Block [VARS] -> Key "NEWASTATE" ”.
A list of
scripts which is loaded at startup of erpcustom.vbb
.
A list of
scripts which is loaded before startup of erpcustom.vbb
.
A list of
scripts which is loaded after startup of erpcustom.vbb
.
The scripts indicated here will be loaded by pressing the button Request ERP number per e-mail .
The scripts indicated here will be loaded by pressing the button Add dataset to link database .