powered by CADENAS

Manual

Manual

2.3.1.4.1. Block [AttributeMapping(is2d)]

In the block AttributeMapping(is2d) you determine whether the PARTsolutions standard attributes are to be exported to the CAD system, and if so, in which language(s).

Under Attr_CopyFrom_00 set the desired language. The keys Attr_Content_00 and Attr_Section_00 remain unchanged.

  • default: The attributes are exported in $CADENAS_LANGUAGE.

  • Assign language (german, english, french, etc.): The standard attributes are exported in the indicated language.

    [Note] Note

    If there is no translation for the given language of the attribute, no attribute will be exported (not even one from the $CADENAS_LANGUAGE language).

  • No entry: No standard attributes are transferred.

In AutoCAD the attributes are available in all relevant dialog windows ("Edit attributes", "Enhanced Attribute-Editor", "Block attribute manager") and in the BOM list.

Attributes in AutoCAD

  • Example 1: Attr_CopyFrom_01 = default

    Example 1: Standard attributes in the Block attribute manager in the default language

    Example 1: Standard attributes in the Block attribute manager in the default language

  • Example 2: Attr_CopyFrom_01 = french

    Example 2: Standard attributes in the Block attribute manager in French

    Example 2: Standard attributes in the Block attribute manager in French