powered by CADENAS

Manual

Manual

4.6.12. PREVIEW

Show or hide the previews of "Animation", "2D/3D", "Technical Details" and "PDF".

[PREVIEW]
;Sets if animation preview is available (as of 1.5)
HideAnimationPreview=false
;Sets if the information preview (technical details etc.) are available (as of 1.5)
HideInformationPreview=false
;Sets if the 23d preview is available (as of 1.6)
Hide23dPreview=false
;Sets if PDF preview is available (as of 1.6)
HidePdfPreview=false

;Indicates if ActiveX is enabled (as of 1.0)
EnableActiveX=true
;Indicates the current used ActiveX viewer version (as of 1.5)
ActiveXViewerVersion=1,0,36,0

;Set if the 2D image preview is used (instead of a plugin -applet or active x) 
;(as of 1.3)
HidePreview2DViewerPlugin=false
;Set if the information image preview is used (instead of a plugin -applet 
;or active x) (as of 1.3)
HidePreviewInformationViewerPlugin=false
;Indicates a preview generation error message (as of 1.3)
HidePreviewGenerationMessages=true
;Sets if the thumbnails are available for the information preview (technical 
;details etc.) (as of 1.3)
HidePreviewInformationThumbnail=false
;Sets if the thumbnails are available for the 2D preview (as of 1.3)
HidePreview2DThumbnail=false

;set to true if the reload frame should be reloaded if
ReloadPreviewFrameOnFolderSelect=true

;Sets if preview should be shown for deep links (as of 1.8)
LoadPreviewForDeepLink=true