powered by CADENAS

Manual

Manual

5.15.2.4.1. Symbols in the Catalogs section

You can filter the directory structure with different methods:

Bitmap

Tooltip at mouseover  

Meaning

Filter tree

In the directory structure everything without update information is hidden.

Hide / Show mapped lines

When you hide already assigned lines, then you can better see, which lines are still to be checked.

Hide / Show lines

When you hide lines, then in fact you have a better overview, but cannot access them.

Example

Example

Symbols in the directory structure:

Changes:

Bitmap

Meaning

The icon with the exclamation mark has the following meanings:

Project or line is found at another position in the new version. See Section 5.15.2.5.3, “Moved dataset”.

Project or line do not exist anymore in the new version. See Section 5.15.2.5.4, “No correlation to the old dataset found”.

Changes approved:

Bitmap

Meaning

Approve assignment
Revoke assignment and save changes

[Note] Note

If several changes apply the respective symbols are overlapping.

Further symbols:

Bitmap

Meaning

An update has been performed without LinkDB connection. See Section 5.15.2.3.1, “Update without connection to the LinkDB ”.

Directory

Project

Line (characteristic)