Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
The following figure shows the default setting.
The ERP_NRGENERATOR key, defines the generator names with the special generating pattern. You can attach as many variables as needed.
The EPR_NRGENERATOR_CONDITIONS key defines the related catalog, directory and project path for every generator.
The following table shows the syntax for the entry of the generating pattern and explains the meaning of the individual values.
Separators between individual values are colons.
In the standard environment two generating patterns (GENERATOR_1 and GENERATOR_2) are defined.
Example value for GENERATOR_1: STD:0:0:5:-std:GEN1
Example value for GENERATOR_2: CAT:0:100:5:-cat:GEN1
Key name | Prefix | Minimum | Maximum | Place number | Postfix | Counter name |
STD | 0 | 0 | 5 | -std | GEN1 | |
CAT | 0 | 100 | 5 | -cat | GEN1 |
The name can be chosen as desired.
Please note that when specifying the path in the ERP_NRGENERATOR_CONDITIONS key, exactly this value is referenced to.
Shows maximum limit for the number generation
For an example value of '5', the '0' is shown as '00000'; the number '101', for example, as '00101'.
The following figure shows an example of a counter as seen for "Minimum", "Maximum" and "Counter name".
Name in order to differentiate between counters in the database table
The following table shows how to configure the requirements.
Separators between individual values are colons.
Requirements depending on roles
You can also define requirements based on user-role dependencies.
[ERP_NRGENERATOR_CONDITIONS(rolename)]
Via the context menu, launch Insert block. Insert the necessary key. Detailed information can be found under Section 1.1.6.3.5, “Edit blocks and keys”.