powered by CADENAS

Manual

Manual

1.1.7.3.  Clients

[Note] Note

Information for existing customers

The following changes appear in the license administration as of PARTsolutions V9.03:

  • A preselection for the license product to be used is available. See Section 1.1.7.3.4, “ "License product preselection" tabbed page ”.

    The setting is not restrictive. The user can modify the setting inside the module.

  • You don't have to determine the hostid to be used manually anymore, because it is automatically detected. Also ports are automatically detected.

  • The "Administrator mode" is cancelled, exactly because no manual settings for the hostid have to be performed anymore.