powered by CADENAS

Manual

Manual

1.1.6.7.21.2. Block [Common]
1.1.6.7.21.2.1.  Key "CADENAS_PRESELECT_LINKDB_GROUP" - Role selection via environment variable

The role selection may be controlled via a system variable as well. The desired role is the automatically selected during registration process, regardless whether the user is configured as valid for this role, or whether he has more than one role available. (The configuration file plinkusers.cfg is irrelevant)

Do the following:

  1. Set a system variable with any name. (For example with the key name CADENAS_PRESELECT_LINKDB_GROUP) and give it the desired value for the role.

  2. Set the key CADENAS_PRESELECT_LINKDB_GROUP onto the desired system variable.

    CADENAS_PRESELECT_LINKDB_GROUP=$CADENAS_PRESELECT_LINKDB_GROUP

[Note] Note

If the key has not been set, nothing happens. If the key is set, then nothing happens either.

Only once the content is in the environment value, the function will be carried out.

1.1.6.7.21.2.2. Key "UPDATESEARCHINDEX"

Update of full-text search index at each LINKDB change:

UPDATESEARCHINDEX= 0/1

Value range: 0/1

In V9.08 the key was used to update the ERP search index once an ERP number had been added. (Locally on the client)

In V10, when adding an ERP number an entry in the LOGTABLE is made. In this way the "Task" on the AppServer updates the ERP search index. Details on this can be found under Section 5.5.6.2.3.1, “Logging of LinkDB changes ”.

That's why, as of V10, the local creation on the client is "off" per default (UPDATESEARCHINDEX=0).

1.1.6.7.21.2.3.  Key "EXPPRJTABLES"

On this see Section 5.21.4.3.2.4, “ Tabbed page "Export tables" ”.

(Extraordinary export release for any 23d-libs directories)